| |
Original Equipment Manufacturers developing machines which require accurate
temperature control now have the perfect answer following the launch of the
new thermo con - Series HEC - from the world leaders in pneumatics and
automation experts, SMC.
Developed initially for the semiconductor industry, Series HEC is a range of
Peltier type chillers which are ideal for ensuring the constant temperature of
circulating fluids. Currently available in either an air cooled – non refrigerant
type - or water cooled options; Series HEC provides accurate temperature
control of +-0.01 to +-0.03ºC. Available in a wide range of power supply
voltages; 100 to 240VAC, 50/60Hz for air cooled models and 200 to 220VAC,
50/60 Hz for water cooled or Galden®HT 135, Fluorinert™FC-3283 options,
this new compact chiller range offers outstanding cooling capacity performance
of between 230 and 1200W depending on the selected model. Further benefits
of the HEC´s Peltier device is that both noise and vibrations are kept to an
absolute minimum.
Series HEC is both CE and IEC 60601-1 Medical Equipment Safety compliant
and the air cooled models are perfect for controlling temperatures in locations
where there are no water facilities.
|
|