| |
Production and packaging applications involving food and beverages often need
specialist equipment to meet the strict hygiene standards required in these
industry sectors. To stop the growth of pathogens and other potentially harmful
agents in this process, efficient antibacterial cleaning is an accepted necessity.
That’s why SMC, the world´s leaders in pneumatic technology, have now
developed a new range of hygienic designed cylinders, Series HY, including a
complementary auto switch ensuring maximum clean-ability.
The complete (HY) hygienic range consists of four model options which all
feature the same smooth, easy to clean, exterior surfaces. Series HYC is a
range of ISO/VDMA approved cylinders with a unique square profile,
non-rising air cushion mechanism, providing improved water resistance and
clean-ability. Series HYG offers increased lateral load performance, Series HYQ
is an ultra compact space saving range and Series HYB, with its round profile
body, finally completes the HY cylinder options.
To complement these ranges SMC have also developed a new rail mounted
auto switch, Series D-F6, which is fully adjustable along the stroke length which
provides improved cleaning benefits by having an intermediate space between
the switch and the cylinder. All the models in the HY range are particularly
suitable for applications in the “non-food” or “splash” zones of a production line
and their high quality construction and special cylinder, food grease, internal
lubrication ensure a lifecycle performance which has never been achieved or
thought possible before.
|
|