| |
Following automotive industry requests for an ATEX approved, air operated
valve for use with either water or chemical based products, SMC - the world
leaders in pneumatic technology - are pleased to launch their new Series VCC
valve range.
With their lightweight resin body manifold construction this new valve range has
been designed for both ease of maintenance and cleaning. Using a simple one-
touch fittings and a clip system it is possible to add or remove a valve without
the need to replace the piping and thanks to its improved sealing, residual liquid
inside the valve is reduced accordingly. Additional benefits of this improved
sealing have also shown in impressive valve performance of up to 5 million
cycles when used with paint and 10 million cycles for air. Fully ATEX compliant,
Series VCC valves are ideal for applications that require the separation of fluids
such as paint and cleaner or pilot air and main fluid.
Designed for use with SMC´s stainless steel fittings range Series VCK, which
includes straight, 40º swivel elbow and 90º swivel elbow type fitting options,
this valve and fitting combination ensures that excellent space saving can be
achieved. |
|