Basket (0)
The Basket is empty
  Quick contact
  Locations
  Rate this page
  E-mail this page
  Print this page

      Press Releases

  Steam ahead of your competition with SMC´s new Zero Differential Valve  
 
 

Industry requests for a competitively priced zero differential solenoid valve for steam applications have now been answered following the launch of the new Series VXS 2 port solenoid valve range from world leaders SMC. Developed with high performance in mind, the VXS range of compact, lightweight, solenoid valves have been designed to operate using minimal power consumption with an operating pressure of 0 MPa. Considerably quieter than similar valves, thanks to their special construction and full wave class H rectifier type AC solenoid valve, Series VXS also uses a pilot type piston to operate the valve which results in excellent steam resistance. Further features of the VXS´s construction include the use of flame resistant moulded materials for the coil (conforming to UL94V-0), the introduction of a special FKM material for both the valve and seal, which has resulted in reduced internal leakage of 1.0cm3/min or less, and improved life cycle and valve reliability. The new VXS valve series is also RoHS compliant and meets IP65 enclosure guidelines. - ends -

 
 
  December 2009  
 
   




  Site Map  |   Copyright 2010  |   Disclaimer/Privacy Policy