SMC, the world’s leading provider of pneumatics, has completed its popular CRB2-Z series with an upgraded version of its free mount, vane type CRBU2-Z rotary actuator.
The CRBU2-Z has a broader range of mounting and positioning options thanks to its clever, lightweight construction delivering improved product performance and functionality.
It’s incredibly easy to mount due to the tapped holes and the through holes in the body of the actuator via the mounting flange, leading to labour cost savings. In addition, the rotary section and flange have been constructed separately, offering various choices for positioning between the mounting flange and the rotary section.
As well as these refined features, the CRBU2-Z series shares the same characteristics as the basic CRB2-Z series. These include the ability to directly mount both an auto switch unit and an angle adjustment unit; plus a double vane construction that doubles the torque. It also has a parallel piping which can be side or axial ported.
The CRBU2-Z is, therefore, ideal for a range of applications including those within small spaces, robotics, material handling, rotary motion, clamp applications and product deviation.
Recognised as a global technology leader and voted for the third consecutive year as one of the world’s most innovative by leading business magazine, Forbes, SMC has a diverse customer base covering all automation industries. For more information about the CRB2-Z Series and the CRBU2-Z in particular, please visit SMC’s New Product Section at www.smc.eu. |