To provide customers with greater energy savings and product choices, SMC
has launched two new designs of its VQC4000/5000 five port solenoid valves.
This launch, which completes the range, gives customers access to greater flow
rates and improved energy consumption.
Vitoria, Spain (May 7, 2015)
Building on the success of its VQC solenoid valve series, worldwide leading
experts in pneumatics, SMC, has completed the range with two new designs.
The VQC4000/5000 give customers ultimate flexibility and cost savings in terms
of energy conservation and operational life expectancy. Greater power efficiencies
have been achieved thanks to a new V100 pilot valve which reduces consumption
to as little as 0.4 W and improves the operating range to 1.0MPa. The new VQC5000
also delivers a flow rate up to 4350 l/min as standard, offering further flexibility
in terms of applications.
Another key benefit of the pilot valve is a built-in strainer in the flow supply
passage which helps to prevent contamination from foreign matter and thereby
extend the operating life of the solenoid valves.
SMC said: “These latest additions to the VQC series underline our commitment
to product enhancement and development. Understanding that cost savings, flexibility
and durability are key drivers for our customers, the VQC4000/5000 demonstrate
we are responding to their needs.”
Suitable for use in general industrial machinery, a new manual locking type
removes the need for additional tools and complements the existing pilot valve
overrides. SMC has also maintained some of the key features of the existing
VQC Series, such as the connector type manifold which makes them so easy to
handle. The addition of a single plug-in, base mounted unit offers further flexibility.
Suitable for use in general industrial machinery, a new manual locking type
removes the need for additional tools and complements the existing pilot valve
overrides. And the addition of a single plug-in base mounted unit leads to offer
even more flexibility. SMC has also maintained some of the key features of the
existing VQC Series, such as the connector type manifold which makes them so
easy to handle.
For more information on the VQC series and the new VQC4000/5000, visit the
SMC new product page: www.smc.eu
|