Product selection
×

Go to details
Part number

My account

×

News

What´s going on?

April 2024

Relief Aid for Earthquakes in Taiwan

We would like to extend our deepest condolences to those who lost their lives in the Earthquakes off the east coast of Taiwan on April 3, 2024, and our heartfelt sympathy to all those affected by the disaster.

Read more

March 2024

SMC receives the “Supplier Excellence Award 2024” from Applied Materials

SMC received the “Supplier Excellence Awards 2024” from Applied Materials, Inc. (herein after “AMAT”), one of the largest semiconductor and display equipment company.

Read more

January 2024

SMC to introduce new EXW1 Series Compact Wireless System

SMC is introducing the new EXW1 Series Compact Wireless System with an increased range of up to 100 m. Similar in technology to the current EX600-W, the EXW1 is smaller, lighter and fieldbus compatible, and with improved features that augment the current portfolio.

Read more
No air source? No problem with SMC’s new compact compressor

The new SMC CRP series compact compressor allows design engineers to take advantage of an innovative product that allows the use of pneumatic components in areas without air source, making it perfect for use in mobile applications. Moreover, designers have the option of using the versatile CRP series as a compressor (positive pressure) or vacuum pump (negative pressure), simply by connecting the pipes in the corresponding way.

Read more
Notification regarding the Earthquake felt in northern Ishikawa area on January 1, 2024

At 16:10 on January 1, 2024 (JST), a huge earthquake with a magnitude of 7.6 struck the Noto region, northern part of Ishikawa Prefecture Japan.

Read more

December 2023

SMC JSY1000-E takes control of valves and ejectors in a single manifold

SMC is once again demonstrating its innovation prowess with the company’s new JSY1000-E valve manifold with fully integrated ejector system. This optimal combination provides a complete solution for positive and negative (vacuum) pressure that allows users to control valves and ejectors in a single, simple manifold. Reducing both physical dimensions and weight, the JSY1000-E also has an energy function available that decreases energy consumption substantially and improves process efficiency.

Read more
SMC JSXF-P controls multiple valves with just one signal

SMC is introducing its innovative JSXF-P series of pulse valves for the effective and efficient dislodging of foreign matter during cleaning procedures. The new JSXF-P SMARTVENT type pulse valve offers a number of notable benefits, including a built-in control board, high peak pressure, low air consumption and long service life.

Read more

November 2023

SMC JSY3000-S valve offers corrosion resistance in food plants

The new JSY3000-S is a bottom-ported manifold with stainless steel plate and FDA-compliant fittings that delivers extended operating life in food and beverage manufacturing environments. Part of SMC’s extensive directional control valve family, the new plug-in JSY3000-S is cabinet-mounted with a robust bottom seal and the piping connections facing outwards. This design configuration helps to protect the valve against both corrosion and splashes from water, ensuring its suitability for location near any type of equipment that requires wash-down procedures.

Read more
New SMC air flow controller combines a flow sensor and pressure regulator in a single unit

SMC is unveiling an innovative air flow controller that combines a flow sensor and electro-pneumatic regulator in a single product. The result for equipment designers and engineers is a space saving of up to 50%, significantly less piping and cables, and reduced installation time. In addition, the new IN502-44/45 allows the precise and reliable control of air flow rate as it is not dependant on piping conditions, pressure differential or temperature. The product benefits any application involving flow control, such as painting, packaging and welding systems across any industry, in particular automotive and food.

Read more

September 2023

Relief Aid for Earthquakes in the Kingdom of Morocco

We would like to extend our deepest condolences to those who lost their lives in the terrible Earthquakes occurred in the Kingdom of Morocco on September 8, 2023, and our heartfelt sympathy to all those affected by the disaster.

Read more
All-in-one solution: electric actuator with integral controller

The new EQ series of slide-type and rod-type electric actuators from SMC feature a fully integrated controller, providing a simpler to set-up, easier-to-use, space-saving solution that simultaneously helps users to save energy and reduce CO2 emissions. As a further advantage, EQ series electric actuators offer straightforward control with simple and exclusive software which helps users to start the actuators working via a single screen in just three steps. First, users choose ‘set operation mode’, before specifying the stopping positions and finally defining the speed, acceleration and deceleration values. It is no more complex than controlling a two- or three-position solenoid valve.

Read more
Boost flow and minimise loss with new SMC angle seat valve

The new JSB series angle seat valve from SMC offers a number of key advantages to OEMs and end users alike, combining long service life, low pressure loss and compact dimensions with a high flow rate. Suitable for use with steam, water and air, optimisation of the JSB’s body flow profile ensures this space-saving valve can deliver the same flow rate as larger counterparts and, in turn, support system energy savings.

Read more

July 2023

SMC receives Bosch Global Supplier Award 2023

The specialist for pneumatic and electric automation SMC got the "Bosch Global Supplier Award" in the category "Indirect Purchasing and Services" for its top performance as a supplier.

Read more
Energy-efficient SMC ZHV vacuum flow delivers benefits in highly demanding applications

All sectors across general manufacturing and automation can take advantage of the SMC ZHV air amplifier, a new product that offers high flow rates which are fully adjustable to suit specific customer requirements. This energy-efficient, compact and lightweight solution functions as either a blow-off or vacuum unit.

Read more

June 2023

SMC will open a new core R&D center in Autumn 2025

We are pleased to inform that SMC will be relocating and expanding its current Tsukuba Technical Center (JTC), and open “Kashiwanoha Campus New Technical Center (provisional name)” in the "Kashiwanoha Smart City" in the fall of 2025.

Read more

February 2023

SMC eyes future gains with strong Business Continuity Plan

As a comprehensive manufacturer of automation equipment, SMC aims to fulfil its product supply responsibilities and maintain the trust of customers by contributing to sustainable growth and the expansion of reliable technological innovations. To help deliver these objectives, SMC has a rock-solid Business Continuity Plan (BCP) that the company is now further strengthening to provide an even more robust automation and motion control offer for its global customer base.

Read more
Donation to support victims of the heavy Earthquakes in Southeastern Turkey

We would like to extend our heartfelt sympathies to all those affected by the terrible Earthquakes occurred in southeastern Turkey on February 6, 2023. And we sincerely hope that the relief efforts will progress rapidly.

Read more

January 2023

Up to 62% less compressed air consumption with next-generation air management hub

Leading industrial automation and IIoT specialist SMC is addressing the need to reduce CO2 emissions and cut energy consumption with the release of its latest innovation, the AMS20/30/40/60 Series compressed air management system. By adopting this revolutionary new air management unit, any company that deploys pneumatic processes can gain from reductions of up to 62% in compressed air consumption, benefiting both the environment and bottom line profitability.

Read more

November 2022

SMC Corporation Recognized Among World’s Best Employers by Forbes

SMC Corporation, a global leader in manufacturing comprehensive automation control equipment has been recognized by Forbes magazine as a World’s Best Employers 2022.

Read more
SMC to introduce new EXW1 Series Compact Wireless System

SMC is introducing the new EXW1 Series Compact Wireless System with an increased range of up to 100 m. Similar in technology to the current EX600-W, the EXW1 is smaller, lighter and fieldbus compatible, and with improved features that augment the current portfolio.

Read more

September 2022

SMC gains listing on Nikkei 225 stock market

SMC, a leading Japan-headquartered global specialist in pneumatic and other automated control solutions, is set to join the Nikkei 225 (or Nikkei Stock Average), the premier and most-often quoted index of Japanese stocks. The Nikkei 225 comprises of 225 stocks selected from Japan’s top-performing and most liquid blue-chip companies. SMC will commence its listing on 3 October 2022.

Read more

August 2022

SMC Statement on Conflict in Ukraine

As devastating, unprovoked attacks continue to unfold in Ukraine, they create a tragic crisis for the Ukrainian people, their families, and their futures. SMC is firmly in opposition to authoritarianism and violence, and we stand in solidarity with the Ukrainian people. We must continue to provide our courageous Ukrainian colleagues with the support they need and are working tirelessly to help our associates who are still in Ukraine, as well as those who have found themselves in the unenviable position of living under authoritarian Russian rule.

Read more
Broaden your range of applications thanks to the new ISE7#/7#G/79S pressure switch

SMC’s ISE7# pressure switch has been updated adding higher pressure ranges apart from offering improved flexibility and higher control of applications, leading to better decision making.

Read more

July 2022

Less wiring and more fieldbus compatibility with new SMC valve/ejector combination manifold

The new JSY & ZK2-A valve and ejector combination manifold from SMC not only simplifies pneumatic systems in applications requiring both positive and negative pressure (vacuum), it also reduces wiring requirements, provides complete compatibility with multiple fieldbus communication protocols and eliminates pressure fluctuations.

Read more
Increased safety and fast communication with SMC step motor controller

Any machine builder looking to simplify and reduce the cost of adding higher levels of safety, while simultaneously seeking faster and broader communication capabilities should consider the new JXCLF step motor controller from SMC. The JXCLF features an IO-Link communication interface and a Safe Torque Off (STO) function, thus presenting machine builders with the opportunity to deliver better control of the manufacturing process and increase their system’s safety integrity level (SIL 3) and performance level (PL e) in a cost-effective way.

Read more

May 2022

New SMC pinch valve ideal for medical and food applications

Leading industrial control and automation solutions specialist, SMC, is adding a new range of pinch valves to its expansive offer for medical device and food system OEMs. With the new LPV series valve, fluid does not come into contact with any moving parts, avoiding the potential for contamination. Moreover, by simply discarding the tube after use, there is no longer any need for a washing process, ensuring good hygiene. SMC’s energy-saving LPV pinch valve is suitable for controlling a wide range of analytical, medical and food industry fluids.

Read more

February 2022

SMC's ZKJ vacuum manifold offers fieldbus compatibility for remote industrial equipment communication

General industrial equipment designers, manufacturers and maintainers can now benefit from the new SMC ZKJ vacuum manifold with PROFINET-enabled communication for remotely controlling and monitoring manufacturing processes. The ZKJ also offers impressive suction flow rate taking its low air consumption and low power consumption specifications into account. Other features include valve protection functionality, IP65 rating and the ability to control up to 16 ejectors with a single manifold.

Read more

January 2022

New SMC valve offers higher performance and control in food plants

The new JSY5000-H valve manifold from SMC is purpose-designed for use in food and beverage manufacturing plants, as well as breweries. Featuring a clean design to cope with regular wash-downs, the IP69K-compliant valve differentiates itself in the marketplace with its high flow rate, low power consumption and IO-Link point-to-point communication capability, bringing a new level of control to production.

Read more

December 2021

SMC launches modular version of digital flow switch for large flow with integrated temperature and pressure sensors

One of the latest digital flow switches to join the SMC family, PF3A#H, monitors the consumption of the main line with a 100:1 ratio. It is IO-Link compatible, and it offers the possibility of being connected to air combination units in a simple way. And now, an even more complete solution can be obtained, thanks to the integrated pressure and temperature sensors.

Read more

September 2021

SMC launches abrasive resistant process pump

A new polypropylene type pump from SMC has been designed to withstand the harshest manufacturing processes, delivering production reliability that lead to cost and energy savings.

Read more

April 2021

Greetings from the newly inaugurated president of SMC

I’m Yoshiki Takada. As of April 1st, 2021, I was appointed as the new president of SMC. Since our founding in 1959, SMC has grown as a comprehensive manufacturer of automatic control equipment, including pneumatic equipment, with the goal of “meeting all of our customer requests”.

Read more

March 2021

SMC launches space saving thermo-chiller

The new HRR rack-mounted thermo-chiller from SMC has been designed for installers where space is an issue. It also delivers efficiencies in terms of installation and maintenance, as it can be adjusted and maintained while installed in a rack.

Read more

January 2021

SMC takes aim with launch of a new gun type ionizer

SMC has designed a new lightweight, handysized ionizing gun that can neutralise static, rapidly and effectively, from a variety of products at different phases of production.

Read more
SMC launches solenoid valve for harsh conditions

SMC has designed a direct operated 2-port solenoid valve that can withstand the harshest of environments whilst saving energy.

Read more

December 2020

SMC launches separate controller bar and nozzle type ionizers

SMC has unveiled the IZT ionizer series that offers customers a compact solution, with a separate controller to optimise space. The new design also offers enhanced monitoring capabilities, the bars and nozzles are simple to adjust, even when located in hard to reach spaces.

Read more

November 2020

SMC launches new energy saving Impact Blow Gun

The new Impact Blow Gun (IBG) from SMC is the most energy efficient on the market, using up to 87% less air than any other standard blowing gun.

Read more

October 2020

SMC launches space saving thermo-chiller

The new HRR rack-mounted thermo-chiller from SMC has been designed for installers where space is an issue. It also delivers efficiencies in terms of installation and maintenance, as it can be adjusted and maintained while installed in a rack.

Read more

September 2020

SMC launches digital flow switch for large flow

The latest digital flow switch to join the SMC family, PF3A7#H, monitors the consumption of the main line with a 100:1 ratio. And now, further benefits come together with IO-Link.

Read more
SMC launches solenoid valve for harsh conditions

SMC has designed a direct operated 2-port solenoid valve that can withstand the harshest of environments whilst saving energy.

Read more

June 2020

SMC launches an all-in-one super silent and energy saving vacuum ejector and pump system

SMC has given its popular all-in-one vacuum unit ejector and pump system a refresh with the launch of the ZK2-A series. The latest incarnation offers customers superb efficiencies in terms of space, energy, maintenance and noise.

Read more
SMC introduces new IN-777 air servo cylinder

For installations that require precise and efficient control in challenging operating conditions, SMC launches its new IN-777 air servo cylinder for multipoint positioning and control

Read more

May 2020

SMC unveils lightweight and high efficient multistage ejector

SMC has renewed its multistage ejector range with the, ZL1/ZL3/ZL6 series, in response to weight reduction demand that comes from the growing use of robotics. This addition to SMC’s vacuum range meets the suction flow requirements for workpieces with high levels of leakage, while also delivering energy efficiencies.

Read more

March 2020

SMC unveils new magnetic gripper for transporting workpieces with uneven or perforated surfaces.

SMC has added to its gripper range with the launch of the MHM, which uses a magnet to handle workpieces. Ideal for workpieces with uneven surfaces or featuring holes, the MHM provides machine operators with reliable and safe handling and reduced cycle times that increases productivity.

Read more
SMC launches new multi-channel digital sensor monitor

The monitoring of multiple lines within a plant has become easier thanks to SMC’s new PSE200A 3-screen display, multi-channel digital sensor monitor.

Read more

February 2020

SMC launches compact type parallel style air gripper

SMC is meeting the challenge of speed and precision presented by the increasing use of robotic arms on production lines with its new JMHZ2 compact type parallel style air gripper.

Read more

January 2020

New Digital Flow Switch Manifold from SMC offers centralised control

A new digital flow switch manifold from SMC simplifies the flow and temperature control of production lines and facilities by housing switches in a single manifold.

Read more

November 2019

SMC unveils new ISO locking cylinder

SMC extends its cylinder range with the launch of its new ISO locking cylinder, CP96N-C96N that has a stronger holding force and is ideal for intermediate stops and drop prevention.

Read more
SMC launches world’s smallest solenoid valve

In response to working closely with its customers and identifying a need for space optimised and cost efficient solutions, SMC launches its JSY 5-port Solenoid Valve with the shortest valve width in the world at 6.4mm.

Read more

September 2019

SMC reveals its smallest compact speed controller to date

SMC has responded to market demand for smaller components with the JAS compact speed controller. Its launch means SMC now offers a complete range of ‘compact’ solutions that also includes cylinders and small integrated auto switches.

Read more
SMC’s digital gap checker is Industry 4.0 ready with IO-Link communication

SMC’s latest digital gap checker, ISA3-L, features IO-Link compatability, offering manufacturers greater control of applications and more information at a glance with its 3-screen data display.

Read more

June 2019

SMC grows European market share

SMC Corporation announces its fifth year of consecutive sales growth for its European business, posting a 6.3% increase to deliver annual net sales of €745.87 million.

Read more

April 2019

On the occasion of SMC’s 60th Anniversary

Yoshiyuki Takada Chairman SMC Corporation

Read more
SMC launches energy efficient air pulse valve

SMC has added to its extensive valve range with the JSXFA, a high peak pressure pulse valve, that is also fast to respond and uses low air consumption, to guarantee energy savings.

Read more

January 2019

SMC in the driving seat with innovative solutions at Tire Technology Expo 2019

TIRE TECHNOLOGY EXPO 2019 5 – 7 March 2019 Deutsche Messe Exhibition Centre, Hanover Hall 21, Booth 9064

Read more

October 2018

SMC showcases life sciences solutions

COMPAMED 2018 12 -15 November 2018 Düsseldorf Trade Fair, Düsseldorf, Germany Hall 8B, Stand H04 Visitors to this year’s COMPAMED will have a chance to view SMC’s diverse range of specialist solutions for the Life Sciences industry.

Read more

January 2018

SMC gets to grip with powerful solutions at Tire Technology Expo 2018

TIRE TECHNOLOGY EXPO 2018 20 - 22 February 2018 Hannover Hall 21, Booth 7045

Read more
SMC makes the grade in the FORBES Global 2000

Japanese automation firm, SMC, has been listed in the FORBES Global 2000 as one of the world’s largest public companies.

Read more
SMC steps up control with its latest multi-axes step motor controller

SMC has extended its multi-axes control step motor controller range, with the launch of the JXC92. This new unit can control up to three electric actuators simultaneously, creating a range of savings and simplifying the process in terms of equipment, wiring, space and programming.

Read more
SMC’s latest centring unit helps to save space and air

The MACM is a new centring unit from SMC that helps to align and position heavy workpieces on the move, so manufacturers can install and operate more compact conveyor lines.

Read more
SMC launches highly adaptable blue silicone rubber vacuum pad

The latest vacuum pad from SMC is the ZP3P, which has been designed to offer optimum absorbing performance and efficient handling. It features a blue coloured, silicone rubber pad that prevents wrinkles and is compliant with the FDA 21CFR§177.2600 elution test.

Read more
SMC merges its digital pressure switch range in 2018 under the same design

SMC is building on the success of its ZSE20(F)/ISE20 pressure switch range that features 3-screen display, 3-step setting mode and selectable delay time function, with the ZSE20(F)#/ISE20# (A, B and C). The extended series will help operators deliver efficiencies in terms of control and time saving.

Read more

December 2017

SMC’s new cylinder with lock unit guarantees easy handling

The MWB Series cylinder from SMC, features a separate lock unit that has been designed with the operator in mind. Versatility and simplicity are key to this latest design with installation and maintenance time kept to a minimum.

Read more
Don’t let static be an issue this winter

Static electricity is an invisible but costly problem for manufacturers that can cause both production issues and lower quality products. This issue can only get worse as winter sets in and temperatures plummet, warns SMC.

Read more

November 2017

SMC launches digital flow switch for large flow

The latest digital flow switch to join the SMC family, PF3A7#H, monitors the consumption of the main line with a 100:1 ratio.

Read more
SMC remains in pole position with enhanced air slide table

SMC has launched an air slide table that is believed to be the most precise, compact and lightweight, offering outstanding performance.

Read more

September 2017

SMC brings solutions to life at COMPAMED 2017

COMPAMED 2017 13 -16 November 2017 Düsseldorf Trade Fair, Düsseldorf, Germany Hall 8B, Stand H04 Visitors to this year’s COMPAMED will have a chance to view SMC’s diverse range of specialist solutions for the Life Sciences industry.

Read more
SMC’s new soft start-up valve cuts energy consumption

SMC, the worldwide leading expert in pneumatics, has updated its AV directional control valve that consumes as little as 0.35W and is suitable for continuous energising.

Read more
SMC rolls out its most compact cylinder featuring a linear guide

SMC, the worldwide leading expert in pneumatics, has launched a compact cylinder with an integrated linear guide. The innovative MXZ Series benefits from using the design of a compact cylinder, coupled with a linear guide that delivers market leading accuracy and linearity.

Read more
SMC’s new 3-screen monitor is latest addition to its sensor family

SMC has introduced the PSE300AC Series to the monitor market. It simplifies the remote monitoring of different types of sensors being used on a factory floor. Thanks to the display colours and screen layout, the PSE300AC allows three different items to be watched at the same time, enabling operators to view the status of applications at a glance.

Read more
SMC’s latest main line filter features high filtration and water removal capabilities

SMC has launched a new stainless steel main line filter with 1 µm nominal filtration rating. The AFF#D Series can remove water droplets without the need for an additional water separator, creating greater efficiencies and space savings.

Read more

August 2017

SMC’s latest valve offers a modular solution for FRL units

The latest VP#17 Series from SMC completes the portfolio of 3 port pressure relief valves for FRL (Filter Regulator Lubricator) units, where electrically operated valves are required.

Read more

July 2017

SMC showcases the right tools for the best performance at EMO 2017

EMO 2017 18 - 23 September 2017 Hannover Exhibition Centre Hall 6, Stand H66 SMC, a global leader in pneumatic and electrical automation technology, will be taking a step into the future as it reveals its tool box of solutions for operators working towards Industry 4.0 at this year’s EMO.

Read more

June 2017

SMC’s launches new air saving speed controllers

SMC has launched two air saving speed controllers that reduce energy consumption and are as simple to operate as standard models.

Read more

May 2017

SMC showcases its unique portfolio of cooling and tempering devices at Laser World 2017

LASER WORLD OF PHOTONICS 2017 26 to 29 June 2017 Munich Trade Fair Centre, Messe, Germany Hall B3, Stand 351 SMC will be revealing its diverse range of cooling and temperature controlling devices that combine both high and constant cooling capacity with optimum cost effectiveness at this year’s Laser World.

Read more
The call to the image is too long and obviously is incorrect

VXB Series, angle seat valve for air, steam and heated water that delivers an extended operating life, low leakage levels and a compact design, now providing an easy visual check too.

Read more
SMC helps customers ‘EXpand’ their communications

The sharp growth in manufacturing automation and the adoption of the Industrial Internet of Things has seen a rise in interest for SMC’s serial interface solutions.

Read more
SMC steps up with full suite of solutions to support every step of the packaging process

As SMC commits to work in partnership with its customers worldwide to drive productivity, performance and energy efficiency, the global automation expert has developed a full range of solutions that have the flexibility to adapt and evolve with its customers’ packaging needs.

Read more
SMC gives the power of motion to customers

SMC customers can feel the full force of its electric actuator range thanks to ongoing investment in its product portfolio that now delivers total movement and control for any application.

Read more
Keeping five steps ahead of energy efficiency

In our 24/7 economy and as Governments and industries battle with our thirst for ever increasing supplies of energy, the global automation specialist, SMC, commits to work in partnership with its customers to drive energy efficiency and reduce wastage.

Read more
SMC Gives Customers Peace of Mind For 2017

Industry is being offered ‘peace of mind’ in 2017 as SMC highlights the opportunity to improve production and ultimately costs through a focus on efficient temperature control.

Read more
SMC raises the bar at drinktec 2017 with versatile solutions

drinktec 2017 11 - 15 September 2017 Messe, Munich Hall B3, Stand 510 SMC, a global leader in pneumatic and electrical automation technology, will be serving up a range of flexible solutions dedicated to the beverage industry at this year’s drinktec from stand 510 in Hall B3.

Read more
SMC’s success continues following investment in R&D and recruitment

SMC, the worldwide leading expert in pneumatics, has recorded another year of growth across its global network, reporting total operating income of €1,187.81 million and net sales of €4,140.72 million [€633.9 million for Europe], an uplift of 3%.

Read more

April 2017

SMC rolls out two new compact cylinders

SMC’s latest compact cylinders, the JMGP guide cylinder and the compact JCQ Series, have been designed with weight and space savings in mind. Both help to reduce machine sizes and costs, and deliver increased efficiency due to their lightweight nature which could enhance cycle time.

Read more

March 2017

SMC unpacks its customer solutions at INTERPACK 2017

INTERPACK 2017 4 to 10 May 2017 Messe, Düsseldorf, Germany Hall 15, Stand D58 Visitors to this year’s INTERPACK will have a chance to view SMC’s energy efficient automation solutions, machine safety components that meet ISO 13849, as well as clean design products for the food industry.

Read more
SMC Launches New 2/3 Port Media Separated Valve

SMC’s new 2/3 Port media separated LVMK20/200 valve series has been designed to prevent armature sticking and corrosion that in the past has led to equipment or valve failure. By preventing fluid from entering the solenoid assembly, it remains pollution free from oil, metal and dust particles, improving overall performance and reliability.

Read more

January 2017

SMC Is The Perfect Component to Drive Exhibitors To Tire 2017

TIRE TECHNOLOGY EXPO 2017 14 - 16 February 2017 Hanover Hall 2, Stand 5088 SMC, a global leader in pneumatic and electrical automation technology, will be showcasing its range of products for the Tire industry, focusing on energy efficiency, machine safety and Industry 4.0, at this year’s Tire Technology Expo.

Read more
Speedy set-up guaranteed with new smc controllers

Two new in-line speed controllers from SMC have been unveiled which are quick and easy to set-up and operate. The in-line type AS features a new push-lock knob, offering simple locking and setting. The AS-FS comes with an indicator that allows for accurate adjustments.

Read more