RoHS Directive 2011/65/EU This refers to the European regulation for the Restriction of the use of certain Hazardous Substances (RoHS) in Electrical and Electronic equipment, which repealed Directive 2002/95/EC. Commonly known as the lead-free directive, RoHS has quite a simple aim: to restrict the use of the following six dangerous substances:
Lead: 1000 ppm or less Mercury: 1000 ppm or less Cadmium: 100 ppm or less Hexavalent chromium: 1000 ppm or less Polybrominated biphenyls (PBBs): 1000 ppm or less Polybrominated diphenyl ethers (PBDEs): 1000 ppm or less. Since the Directive took full effect in 2006, at SMC we are actively working to gradually adapt all our products to it. You can view all of SMC's RoHS-compliant products here.
RoHS compliant products are indicated by the symbol [G] on the product and packaging labels.
SMC recognises that the conservation of the earth's environment is one of the most important challenges facing the human race and that our contribution is to develop and supply environmentally-friendly products.
This commitment is translated into the following seven principles:
The above shows our interpretation based on legal regulations as of August 2017. Customers purchasing SMC products for use in RoHS-compliant equipment should study the Directive to understand their legal obligations.