By Philippe Pinto – Industry Manager Life Science, Europe
 
  Who has not heard about the PCR test? In vitro diagnostics (IVD) in general and analyser in a more specific sense, have always played a key role in society as they are non-invasive tests performed on biological samples (for example blood, urine or tissues) to diagnose or exclude diseases. Covid-19 has put IVD in the spotlight and diagnostic tests are, unfortunately a normal part of our daily conversations. The professionals in IVD already knew that an early diagnosis can make the difference; that the right diagnosis can make the difference. Now we all know. In this context it is no wonder that a key target for IVD in general, and analysers in particular is for them to provide fast results as well as accurate ones. Appropriate fluid handling of these techniques plays a fundamental part in achieving the desired speed and accuracy. As fluid handling involves many critical components interrelating together, it is vital to involve a skilled partner able to supply proven solutions for the entire system, at early stages of development. And that´s SMC.
 
  In the land field of analysers
 
  Let’s define what is an analyser. This is an instrument or device that conducts chemical analysis on samples or sample streams to provide haematology values (e.g. red blood cell count, haemoglobin concentrations) or to determine the concentration of analytes (e.g. cholesterol, glucose). This capability assists in the diagnosis and treatment of diseases that include e.g. diabetes, infectious diseases, oncology, diabetes, anaemia, autoimmune deficiencies, cancer and hepatitis, drug testing HIV/AIDS, and of course Covid-19.
 
  There are three common types of analyser: 
 
   
   - for clinical laboratory testing
  
   - for near-patient testing and
  
   - for self-testing. 
  
  
 
  Optimising fluid handling as the key part to ensure the desired speed, repeatability and accuracy
 
  Whatever the testing technologies – e.g. clinical chemistry, haematology, immunoassay urinalysis, DNA, biology, molecular – the fluid (liquids or gases) handling system have a critical importance as it contributes to ensure desired speed, repeatability, and accuracy of an analyser. These complex systems handle the sample extraction, the mixing with reagents, the introduction into the analyser and finally washing of its own circuit. In this context, it is crucial to select a supplier with a complete and proven range of solutions.
 
  The challenge of addressing speed and repeatability
 
  One of fluid handling’s main technical challenges is the interaction among the given functions. This fact creates a situation where an increase in the speed could endanger repeatability. The combination of speed and pressure may affect the test precision as the speed increases the risk bubble generation or turbulence which affects the repeatability. The selection of the optimised designed components with for example, minimisation of dead volume, or circuit topology optimisation, minimises these problems without leaving a side to choose the right compatibility material in contact with the fluid.
 
  Ensure no sample contamination with the appropriate fluid control to help enhance analyser speed and reliability
 
  On an analyser, the isolation valve controls the on/off function and flow path direction for different functions, from fluid sampling circuit to waster line circuit. This valve manages the flow of bleach or saline wash solution that cleans the test equipment’s tubing, as well as the end probes of pipettes and pumps before a new sample can be analysed.  So, minimising the dead volume to ensure no contamination is vital. 
 
  Isolation valves’ most important feature is the diaphragm in EPDM, FKM or FFKM, the rest if the wetted part is in peek which completely isolates its internal parts from the analyser’s flow path to mitigate the risk of contaminating the process fluid. Notably, the space between the valve’s internal chamber and flow path is purposely constructed to minimise dead volume, where trapped chemicals could carry over to the next test’s fluid flow when the valve is closed and re-energised. 
 
  The internal flow path of an isolation valve from SMC is notable for its smooth surfaces, preventing the generation of bubbles and other flow concerns. SMC offers proven, high-quality solutions with a large internal volume, all backed by specialist sales teams. A large range is available covering many options and sizes. Central among the features of SMC isolation valves is low power consumption to avoid any heat transfer to the fluid.
 
  Ensuring repeatability, no contamination and efficient fluid mixing and dosing through customised acrylic manifold
 
  An acrylic manifold is a multi-layered bonded manifold, and is equivalent to a printed circuit board, but for fluids. It ensures that the sample and reagent are introduced in the analyser in the right proportion. This solution should be preferred to the tube-to-tube connections for performing analysers as it offers many advantages. For example, an acrylic manifold greatly reduces the number of joints, thus combatting common analyser issues such as leaks and tampering with tubes, which results in better repeatability. 
 
  These solutions also reduce the overall size of the fluidic assembly, saving space in a very crowded analyser, while a further benefit is the provision of easy visual inspection to check for flow path contamination, for instance.