Productos seleccionados
×

Ir para detalhes
Referência

Minha conta

×

"The results obtained have been palpable to our customers right from the start. The most visible aspect is the better treatment of the textile and the increase in ironing processing cycles. However, optimising the pressure produced another set of benefits such as cost reduction arising from electricity savings of up to 30% and a reduction of up to 25% in air consumption.", explains Quim Riera